Hi, I would like to know if ST25RU3993 UHF Reader can read any type UHF Tag. In selecting different types of UHF tags is it enough to verify the PROTOCOL alone or should we check any other factor?Thanks in Advance
This is the related page: https://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/st25-nfc-rfid-eval-tools/st25-nfc-rfid-antennas/ant7-t-st25dv04k.html
Should we have to necessarily use the RFAL library ? If not than can anybody tell the basic configurations of registers so that ST25R3911B detects TYPE-A card.
Hi,I have purchased ST25RU3993-EVAL board with complete set and I am able to read tags. I would like to know if I can interface this board - RFID Reader with another micro controller (I wanted to interface with TI CC1352P1 launchpad), via SPI (or via...
Hi , After starting power supply , without any configuration od ST25R3911B, can we directly read the "IC Identity Register 0x3F" just to check the SPI with the controller is working or not ? Will it give the value specified in the datasheet or should...
Hello,in the datasheet of the M24LR64E-R is provided the internal capacitance of the M24LR64E-R for an SO8 package.Do you know what is the capacitance for the TSSOP8 package?Thank you,Mattia Berton
I have ported the ST25DV NFC tag driver from STM SDK for TI's CC2650 SoC. Currently, I am able to successfully read and write TEXT data to the tag via I2C. However, when I read the data out from the tag using the STM's NFC Tap APP, I see that the da...
Hi Community, this is my first post here.I was wondering if there is a way to get the previous releases of the CUBE-NFC03A1 libraries (1.4.0 and lower). In fact, I want to use the Ndef_lib examples which are not supported anymore in the latest versio...