Other: hardware

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Questions about MLPF-WB55-02E3 PCB assembly

Hello. I going to use MLPF-WB55-02E3 with STM32WB55V WLCSP_100.1 On the datasheet MLPF-WB55-02E3 there are recommendation for PCB assembly this chip. The document prescribes to use ground CPW line (on antenna side) with sizes as in the pictures Figu...

0690X00000DBqsxQAD.png

select Rbus versus Cbus Value (M24M01)

Hi,I'm trying to develop using the M24M01 product. There is a part in DATASHEET that I don't understand, so I leave a question.In the item 'Maximum Rbus value versus bus parasitic capacitance Cbus', it is stated that the Rbus X Cbus value should come...

yjin.1 by Associate II
  • 497 Views
  • 3 replies
  • 0 kudos

SPEAr(1340) USB Flashing utility

I need the most recent version of the SPEAr USB Flashing utility that works with SPEAr1340. Version 3.2.5 is listed on st.com but the download is decidedly not the USB flasher. The previous version download, v2.4, does download but doesn't work with ...

CBoyd.1 by Associate
  • 264 Views
  • 0 replies
  • 0 kudos

M95M01-A125 in half duplex mode

Can the M95M01 work in half duplex mode? The Master has a 3 wire SPI interface with one open drain DIO. From the timings it looks like the M95M01 output is in high impedance whenever the master is accessing the bus. When the slave is answering the ma...

gcele by Associate
  • 215 Views
  • 1 replies
  • 0 kudos

Resolved! Applying voltage to the output pin of STMPS2171STR

Hi,Currently, I have two boards that contain a 5 volt power supply. Due to flexibility for future projects, both of are powering the same pin on a connector. The STMPS2171STR was added to one of the boards to cut the voltage going to the connector. H...

MOliv.1 by Associate II
  • 660 Views
  • 7 replies
  • 0 kudos

Truth Table for STHV800L?

Hi,the included data brief in ST site does not provide the function of input pins. Like a truth table as to how to control different channels I was wondering if someone can provide me with the same..Thanks in Advance.Thanks and Regards,Siva

SSR by Associate
  • 194 Views
  • 1 replies
  • 0 kudos