cancel
Showing results for 
Search instead for 
Did you mean: 

Does the Teseo module contain anything that can raise the noise floor below 200MHz?

Antypas.Peter
Senior

I can't find any forum for the Teseo so I'm asking here. I need to know if it's appropriate for a very sensitive receiver in the sub-200MHz range. If the module contains any DC/DC switches that raise the noise floor in these frequencies then it's a non-starter for my project.

Furthermore, because of the mechanical size constraints, proximity of the module to the RX chain of the circuit is non negotiable, so I can't just redo the layout to move it away.

0 REPLIES 0