Other: hardware

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPEAr1310

Good morning, I should reprogram a "SPEAr1310" do you have any device that does this?Thank you.

loris by Associate
  • 220 Views
  • 0 replies
  • 0 kudos

ST33KTPM2X32CKE3

Pl suggest the Maximum Junction temperature of ST33KTPM2X32CKE3 and ThetaJa (k/W)

SKCL by Associate
  • 215 Views
  • 0 replies
  • 0 kudos

Resolved! STUSB4500 PDO SRC not read

Hi,I have a custom PCB with STUSB4500 as the UCPD controller and STM32H7 as my application processor. Without any I2C communication between stm32h7 and stusb4500 the stusb4500 is able to negotiate a higher voltage from a usbC PD source by matching it...

rd1987 by Associate II
  • 890 Views
  • 4 replies
  • 0 kudos

Identify IC

Where can I buy this IC? I can't  find any information for it. If it is obsolete can you point me to the datasheet and alternatives?

image.png
bmateev by Associate
  • 302 Views
  • 0 replies
  • 0 kudos

PM8805 POE PD not working over negotiation

We have used PM8805 tr POE PD IC. And design is very similar to one of the evolution board. Its not showing any LED for T0, T1, T2. It looks like its just in the negotiation stage. Please check the schematic and advice us to fix this issue. Thanks. P...

Question about ASM330LHH: reading and writing problem

Good morning, I have some doubts about the functioning of the ASM330LHH. I can read the device id 0x6B, but only if I send this code: Fig1Why does it work for me? the data should not be written this way? Fig2The microcontroller I'm using is an SPC58t...

fig1.png fig2.png
GJord.3 by Associate
  • 231 Views
  • 0 replies
  • 0 kudos

STP8NK100Z Pspice model

I am exploring and experimenting  with the power MOSFET part number- STP8NK100Z. I want pspice models for this MOSFET. Any help is welcome.

Vikram1 by Associate
  • 292 Views
  • 0 replies
  • 0 kudos