Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

how import git project?

how to import this project: https://github.com/lucysrausch/stm32-turbotronik ?I test importing with (EGit - integration for Eclipse 6.7.0) extension from Eclipse market, but not success (Build icon is not active) same if importing from local director...

kliurka by Associate II
  • 1700 Views
  • 8 replies
  • 5 kudos

Resolved! how to power a 24volts electromagnet

i am using electromagnetic sensor which is 24volts. in that i only have the connections for power voltage(positive) and the signal. when i am trying to power it with my stm32f411re nucleo board i can see that the power isn't sufficient. so can i use ...

suhfi by Senior
  • 4411 Views
  • 21 replies
  • 6 kudos

EEPROM (M95P08-I) Safety register

Hi , I am using an M95P08-I SPI EEPROM . And I can now write/erase/program the EEPROM successfully. But I tried reading the Safety register format (RDCR) and found that the Power-up flag (PUF) bit and the Erase flag (ERF) bit were 1.Aften  tried usin...

1123 by Associate II
  • 464 Views
  • 0 replies
  • 0 kudos

DMX512 with stm32F103

i am trying to receive DMX512 signal on my stm32F103 Board but initially i just wanted to see if the interrupt is working , but it did not , so i saw if there is any Framing error but the SR was 192 , which suggests that there is no errors in the fra...

Aniket by Associate II
  • 464 Views
  • 1 replies
  • 0 kudos

Resolved! Connecting from 5V sensor to 3V3 adc channel

Hello everyone,I want to make an adc reading using STM32F103C8T6 but I am really confused. first of all, the sensor I will use is the hall effect open loop current sensor ‘L31S300S05FS’ model. this sensor has 4 pins VCC GND VOUT VREF from these pinsV...

Screenshot from 2024-10-02 17-57-23.png Screenshot from 2024-10-03 10-50-57.png
FinFet by Associate II
  • 1065 Views
  • 4 replies
  • 2 kudos

doubt memory chip hdd bios

1) I spoke to a hard drive specialist and he said that the BIOS of 2.5" and 3.5" HDDs is recorded on these memory chips but I don't know what type of memory and retention timethe models:The 8pins (4 pins on each sides) with 25P05VP、25P10VP、25F512、25F...

ÍStef.1 by Associate II
  • 1654 Views
  • 10 replies
  • 0 kudos

Resolved! Use of EV-L99LDLH32GEN development board

1. Regarding the development board: Does EV-L99LDLH32GEN require an external driver to work? Or does the development board come with its own driver chip? 2. In addition to driving LEDs, can it also drive other loads?   This post has been translated f...

Jing_H by Associate
  • 425 Views
  • 1 replies
  • 0 kudos