The old M95256-W datasheet Rev. 6 says:"The M95256-W and the M95256-R devices (2.5V and 1.8V versions, processed in F8 andidentified with the letter "A") offer an ECC (Error Correction Code) logic"The new version Rev. 21 says:"M95256 and M95256-D dev...
Does anyone know where I might be able to find PSDPRO programmer and WS6102 socket? I need to program an PSD301.I have UV windowed PSD301 it erased well.tried with my 3rd party universal programmer but failed to wrote.somebody help me..Thanks.
The application is a solenoid driver, 12V 0.5A running PWM 1Khz. It's a very basic low side application, diode across the coil. The signal is 5V logic from a microcontroller.I have read the datasheet, and the application note AN4798. to be honest som...
[17:13:18.309]ÊÕ¡û¡ô+WIND:1:Poweron:171117-0328fe3-SPWF04S+WIND:13:Copyright (c) 2012-2017 STMicroelectronics, Inc. All rights Reserved:SPWF04SC+WIND:65:Factory Reset:1+WIND:0:Console active+WIND:3:Watchdog Running:20[17:13:19.307]ÊÕ¡û¡ô+WIND:32:WiFi...
This is debug setting in my project.http://www.keil.com/support/docs/3902.htmAlthough I'm doing this instruction but not working.