cancel
Showing results for 
Search instead for 
Did you mean: 

Currently working with M95256. I am doing a single byte write and making the assumption that I do not need to check the WEL bit in the status register, having written the WREN register, before undertaking the write cycle.

WWyat.1023
Associate
 
1 REPLY 1
Pierre P.
Senior III

​Hello,

Up to you to check or not the WEL bit before the internal write cycle.

You can also check it when you monitor the WIP bit during the Tw.

BR

EEPROM suPPort Team