The old M95256-W datasheet Rev. 6 says:"The M95256-W and the M95256-R devices (2.5V and 1.8V versions, processed in F8 andidentified with the letter "A") offer an ECC (Error Correction Code) logic"The new version Rev. 21 says:"M95256 and M95256-D dev...
Does anyone know where I might be able to find PSDPRO programmer and WS6102 socket? I need to program an PSD301.I have UV windowed PSD301 it erased well.tried with my 3rd party universal programmer but failed to wrote.somebody help me..Thanks.
The application is a solenoid driver, 12V 0.5A running PWM 1Khz. It's a very basic low side application, diode across the coil. The signal is 5V logic from a microcontroller.I have read the datasheet, and the application note AN4798. to be honest som...
[17:13:18.309]ÊÕ¡û¡ô+WIND:1:Poweron:171117-0328fe3-SPWF04S+WIND:13:Copyright (c) 2012-2017 STMicroelectronics, Inc. All rights Reserved:SPWF04SC+WIND:65:Factory Reset:1+WIND:0:Console active+WIND:3:Watchdog Running:20[17:13:19.307]ÊÕ¡û¡ô+WIND:32:WiFi...
This is debug setting in my project.http://www.keil.com/support/docs/3902.htmAlthough I'm doing this instruction but not working.
Hi, going through the ST Micro spec (PCN AMS-APD/12/7174),the ST Micro reel label example lists under "Type", there could be two parts numbers with one representing commercial product and the other one representing the finished goods (see below image...