I want to know in "ST6210C" controller, IS "Data RAM (084h-08fh)" has non volatile memory ? If it is not, then please tell me which memory space in "ST6210C" controller is non volatile ?Regards,Hitesh
I am trying to obtain the gerber data for the above device on here, but cannot seem to find it, I have the recommended footprint pad size, but want to see how the device has been tracked away from the 0.19mm pads
The pinout of the connector and USB controller I am using means that I need to flip the differential signals either side of the ECMF4-20A42N10.The layout would be a lot cleaner if I could swap D+/- signals on this device. For example:Swap Pins 9/10 a...
I attached a photo of the chip.-SOIC-8-Reads "358"-Then reads "ST EZ707" could also be "ST EZ7D7" or "ST EZ7B7"Thanks for the help.
We have made good progress in migrating from an ST90R158 (ROMLESS) processor to an ST158E158 (EPROM). The issue we are now facing is that the code that is running in the ST90E will not run in the ST90T (will not even try to boot), which is our ultima...
MTBF details along with test temperature, confidence level and fit values.
I need the documentation to go with the libraries too. I have inherited a project based around the STR912FAW44X6 which needs to be changed. It looks like I need V2.1 (12/22/2008) . We have plenty of stock, and no time to re-design at the moment.