Others: hardware and software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Datasheet of XRU8871

Hi,During the holidays, my dad asked me to fix an old device of his. There doesn't seem to be any visible damage (eg. leaking caps or corrosion on the PCB), so I wanted to check if all the ICs on it are still functioning correctly. However, for many ...

0693W00000HqQ8cQAF.jpg

The idea of creating debug microcontrollers, in which the pins would have set-diodes that would display the process of data exchange.

I had an idea for debug microcontrollers, so that there were microcontrollers with a light display of the receive-transmit channel. Such chips will be in the category of debug chips, when a circuit is being developed and it is much easier for the cod...

0693W00000GZH6ZQAX.jpg 0693W00000GZGuoQAH.jpg
ssm by Associate II
  • 1193 Views
  • 9 replies
  • 0 kudos

How to use the buck switching regulator ST1S03PUR, and dimension the components value for an out 3v3 and 500mA?

Hi, latelly I am trying to use the buck switching regulator ST1S03PUR and I have some problems with it. It should be something easy to do but seems like not.I have a DC Vin 12V and i want as out 3V3 and 500mA.For the Vout I am using the formula from ...

LUruc.1 by Associate II
  • 833 Views
  • 4 replies
  • 0 kudos

M24C04-DRE

I saw two version of subjected item at EE marketing , ​ is different on body marking , one is 404RP, the other is 404RB, so I would like to know the distinguish between them on electrical parameter? can alternative to use?

AJian.2 by Associate
  • 1082 Views
  • 3 replies
  • 0 kudos

ECMF02-2HSMX6 - Change D+/D-

Hello ST-Community,we are using the ECMF02-2HSMX6 in our USB3.0 application for ESD protection. Is it possible to change the D+ and D- lines? Internally, the part should be electrically the same, but it is not mentioned.Thanks a lot Holger

HKapl.1 by Associate
  • 527 Views
  • 1 replies
  • 1 kudos