Hi, I'm using some VNQ5E160AK with current monitoring. According to datasheet Iout/Isense ratio is in the range of 465 for 'high' current, means it should be 6.5mA for 3A and 21.5mA for 10A. As my ADC range is 5V, I load sense pin with a 200 Ohm resi...
Hello,we are using STR73x device. Our application needs to get 1 ADC sample every 5 ms and uses DMA to transfer that to memory.to do this, we setup a TB1 timer to trigger every 5 ms.On TB1 interrupt, we start a single shot ADC conversion.This works ...
I have BK Precision 864 universal programmer. Can I use it to flash this MC? Or please let me know what hardware (cables, prorammer hardware etc) is needed if I use PSDSoft software.
We have used Wifi Module “SPWF01SC�? in one of our projects. Now recently we are getting more issue in wifi module.Most of the modules are not responding to AT commands. Can you please suggest possible troubleshoot steps to resolve this issue.
Hello,I want to connect esp8266 wifi using stm32f4 to an access point, I find that the module is not stable; sometimes it connects and sometimes no, I didn't understand why. can someone gone through that please help me?here is my code and thanks in a...
I want to know the gate length and channel length of STF23N80K5 and STF26N60M2?This is for neutron affect analysis in space environment.
I cannot find any data on these and the part is obsoleteThanks George
Hello. I'm designing a new board where I use VNI8200XP to control some LEDs and relay loads.In my case VNI is used in SPI mode (SEL2 pulled high to Vreg), internal DC/DC converter is disabled and Vreg is supplied from on-board +24V/+5V DC/DC Converte...
Hello, can more of STA310 datasheets can be shared now. Eg. application manuals or example code, firmware and so on?