Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Does STM run in HALT0 mode?

Posted on February 14, 2017 at 10:39Hello,Our application on the SPC560P44L3 switches to HALT0 mode in the idle loop for power saving. The PIT is configured to wakeup the CPU every msec for handling timers, which works just fine.Now I'd like to conf...

C++ constructor of static objects not called

Posted on February 08, 2017 at 14:18 Hello, I am trying to use C++ in the SPC560Bxx mcu using SPC5 Studio and the free gcc vle toolchain (4.9.2). However, it looks like constructors aren't called as I expected. In the following example, ...

SWT interrupt

Posted on February 09, 2017 at 16:15Hi,I'm having problems with the SWT generating an interrupt before going through reset on the SPC560P44L3ITR bit is enabled, and when I trigger the watchdog I see the TIF bit switch on after the first timeout, and...

[ATT]7360

Posted on February 07, 2017 at 14:41 Title Document: ChibiCubeHello to everyone, I am Rocco Marco and I am going to introduce ChibiCube v2.0.http://www.youtube.com/watch?v=L2IVJro_tqs ChibiCube is a project realized by two trainees thanks to the tec...

Resolved! Initialization MCU

Posted on January 22, 2017 at 12:34 Good day. This my first application on spc5 studio. I add for testing one led on Port B[1] to board witch MCU SPC560P40L3. I add in generate main.c file one sting -pal_setpad(PORT_B, LED_RED);. Pin will add p...

0690X0000060Mq1QAE.jpg 0690X00000603SwQAI.jpg 0690X00000603SxQAI.jpg

Impossible to download SPC5Studio

Posted on March 23, 2016 at 09:29Dear All ,there is a bug in our lovely corporate website.it is not possible to download SPC5Studio by http://www.st.comour IT is trying to solve the issue as soon as possible.             Best regards                ...