Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Problem with ADC on the Bernina

Hello,I've got a problem with max analog channel input voltage. When all supply voltages are 5V everything is fine. But if VDD_HV_IO_MAIN voltage is 3.3V while VDD_HV_ADV is 5V, the analog channel input voltage becomes limited over 4V. This problem i...

download.spc5studio.com

Important Upgrade : SPC5Studio 5.8.1 is availableDear All ,SPC5Studio 5.8.1 is availableNew or updated componentsCore 1.2.0Mass Market:SPC5Studio multi update site components management (see above).Flash 1.7.0Selected Customers:Flash driver for SPC58...

SARADC driver activated but no SARADC peripheral assigned

Posted on July 11, 2018 at 20:07Hello all,I am using SPC570s-Disp eval board and I want to activate the SARADC lld's. I have selected it in the Low Level Drivers Component RLA page, as shown in the screenshot. However, in the MCU wizard tool, it is ...

SARADC_0 ICNCMR problems

Posted on July 11, 2018 at 11:45Hello everyone,I have an SPC57S-Discovery eval board. I am trying to use both SARADC_B and SARADC_0 modules concurrently so that I can sample and eval from two channels at the same time. The code is given in the attac...

Resolved! SPC5Studio example application Error: Cannot load configuration file 'L/SPC56ELxx_RLA ADC Test Application for DiscoveryPlus/configuration.xml':

Posted on June 30, 2018 at 04:28Hello (I am new to ST and SPC5Studio)I just used the SPC5Studio Application Wizard to import the SPC56ELxx_RLA ADC Test Application for DiscoveryPlus and when I tried to generate it it showed the following error:Error...

SPC5Studio at EclipseCON 2018

Posted on June 29, 2018 at 16:10 Title Document: SPC5Studio at EclipseCON 2018EclipseCon France 2018https://www.eclipsecon.org/france2018/session/embedded-automotive-applications-are-just-few-clicks-away Speaker(s): Philippe Noel (STMicroelectronics...

download.spc5studio.com

Posted on June 29, 2018 at 15:41Runtime IO Component is available (1.1.0) Dear All ,Runtime IO Component is available for SPC5Studio 5.8.0.What is Runtime IO Component?The Runtime IO Component allow you to use the standard printf function to write a...

github.com

Posted on June 25, 2018 at 10:11Rt-Thread for XPC56(only support E200Z0) web:     https://github.com/snikeguo/rt-thread/tree/master/libcpu/ppc/E200Z0 If you have any questions, please contact mailto:snikeguo@foxmail.com.thx. #rtos