Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Unlock JTAG programmatically by code on SPC58

Hi, I'm developing a Bootloader for SPC58, If I full secure the micro and put its LC status as In-Field on UTEST, is there a way from the internal code (I can implement a serial command for the purpose) to unlock the JTAG? Or there is no way animore?...

GMG by Associate III
  • 142 Views
  • 2 replies
  • 0 kudos

stellar studio

我能为此问题做些什么 似乎系统无法使用 SDKS 文件夹中的工具 Translation: "What can I do with this problem? It seems that the system cannot use the tools in the SDKS folder"  

200c99ebacd1084d0572e3e94abd71ef.png
zi_n by Associate
  • 122 Views
  • 1 replies
  • 0 kudos

SPC5Studio SPI Generating Code for SPC574K not working

Hallo,I tried to use the DSPI_0 interface with the transfer configuration as shown in the picture, but cannot generate the necessary code with the error shown below. I could try a walkaround with byte wise frames and exchanging 4 bytes at a time but ...

grafik.png

Setup Output Pin for SPC582B PWM Emios

I want to generate pwm signal with spc582B with out the signal directly to pin emios0 channel 11 (uc11 pin).Already use the pwm Icu sample project. With channel 11 out, so I use group 1. When running, the periode callback is working, but still no out...

jmary by Associate III
  • 97 Views
  • 0 replies
  • 0 kudos

SPC58EC BMS Project : PIT Timers

Hello,As part of a custom BMS project, I am trying to add a cyclic CAN Message Transmission functionality to the board. I have been able to implement CAN transmission functionality on the main_core0 function where a function is called after every 500...

Vipuls by Associate III
  • 107 Views
  • 0 replies
  • 0 kudos

Changing start address at 0x011C0000 flash area

I’m trying to implement FOTA on SPC58NH, and changing the application start address is causing some issues.The 0x011C0000 flash block is not included in the boot record search locations.So I need to make the core start from this address, but I failed...

JYKim by Associate
  • 96 Views
  • 0 replies
  • 0 kudos

Resolved! Multi-core debugging on SPC58

I have been using SPC5-UDESTK with a STM58 evaluation board. I now need to start working with multiple cores, but it appears that the starter kit license does not support this functionality. Will the SPC5-UDEDEBG license allow for multi-core debuggin...

nullptr by Associate
  • 180 Views
  • 1 replies
  • 0 kudos