Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

LINTCSR of SPC560P34L1CEFA

Posted on November 06, 2017 at 01:37After MCU reset, I got the following and the IOT bit is set. But according to the RM0046(Reference manual, September 2013, Rev 5) the IOT bit should be reset after MCU reset.#lintcsr

0690X00000604C0QAI.jpg 0690X0000060497QAA.jpg

Resolved! Is the cloudforge server still used for updates?

Posted on November 09, 2017 at 02:11I downloaded the latest SPC5Studio version 5.5.  If I check for updates, it looks for http://spc5.drive.cloudforge.com/projects/spc5releases/spc5studio/updates5 which does not exist.  The root branches for SPC5Stu...

Does BootLoader have to run in RAM For SPC5XXX?

Posted on September 23, 2017 at 09:29I have a board of SPC560B. I need to make a BootLoader.I want to do that:the JMP_ADDRESS is 0x40000PowerON--> running BootLoader at 0x000000 in flash.--->delay 3000ms-->if (update cmd ==false)----->  (*(AppFu...

Generating variable frequency PWM on SPC570s

Posted on October 27, 2017 at 07:17Dear AllI am trying to generate the variable frequency PWM on SPC570s using Evaluation Board following the documents'SPC570Sx 32-bit Power Architecture�microcontroller for automotive ASILD applications'page 759 Usa...

MPU variants

Posted on October 22, 2017 at 00:36Hi,in the en.DM00293238.pdf document, CMPU and SMPU are shown for spc58ec80. Other documents relating to the e200z4d mentioned only MMU in core (no mpuwe instruction and mpu related registers shown) and only system...

Flash drivers for SPC56 L line

Posted on October 20, 2017 at 12:19Flash library for SPC56xLHi,I need to develop my own bootloader for SPC56EL60 microcontroller, I downloaded the flash library from SPC5 Studio, but in the Flash .c source  files I see only const unsigned char value...