User Activity

Posted on June 11, 2018 at 10:15I feel like I am not finding an explicit answer to this question in the errata.  I notice that the SPC56 has a 5V tolerant ADC, but I am wondering if I can use 5VDC logic for the GPIO pins?  I have some legacy 5V shif...
Posted on April 30, 2018 at 22:24I have DO-160 testing to do on some avionics units.  This certification is destructive, and I frankly do not know if the SPC will survive the MOPS in my particular application.  A lot of this is empirical [not analys...
Posted on March 23, 2018 at 09:21I don't think I have a timer enabled.  I don't see the WDT setting in the outline, but in the configuration.xml it is disabled.  Most importantly clock_cfg.h is  generated as '#define SPC5_DISABLE_WATCHDOG           ...
Posted on February 23, 2018 at 10:14I have a DPM configuration for SPC56EL70.  I initially had some trouble getting the debugger to connect to the target ( could connect fine in LSM.)  The problem had to do with not clearing the LSM_DPMB bit.  Erwan...
Posted on February 20, 2018 at 08:36I am wanting to run in DPM .  I use SPC5Studio to create a .wsx configuration to debug with, but I get the following failure when I try to connect to the target:----------------------------------------------------...