Hi everybody!I working on a simple project but with some sensors and co.I'm newbie with the STM32 and I want to try to port the project from the ATmega2560 to the STM32.But witch chip? I need :> SPI for an TFT screen 2.2" (ILI9340C or ILI9341)> SPI f...
For an application we are investigating this processor and have two questions,We want to connect an external chip to the FMC bus. It is somespecialized ASIC handling some real-time communication.I don't see the option in the STM32Cube to active the F...
Hi,I have succesfully built a image st-example-image-qt from the DISTRO openstlinux-eglfs.I have deployed the image on sd card, and played it on STM32MP157C-DK2.System is booting without a problem, and the splashscreen was shown.Then, I tried one of ...
HiI got an STM32MP157C-DK2 during the Embedded World.But Windows7 isn't detecting the DFU ... It detects only the STLink (UART) ....Same issue in a Ubuntu-16 (which is running in VirtualBox on the same Windows 7)Any suggestion?Regards Francesco
Hi,I'm planning to buy an STM32MP1 discovery kit (when available) and I'm wondering how to get access to the distribution package. I read on wiki.st.com that I have to request these rights to my ST support contact but I can't found out how to do it.T...
I downloaded Yocto_SDK Software Version- 1.0.0 for STM32MP151C. The environment setup file name is - "environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi". Does it mean that this SDK is tailored for Wayland implementation? We i...
Hello,until now, all STM32 datasheets do not specify JTAG/SWD interface characteristics except for STM32H7: 6.3.33 JTAG/SWD interface characteristics.The JTAG/SWD interface characteristics should be specified.