STM32 MPUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP1 ethernet issue

Hi,We are using the STM32MP157CAA3 SoC in our design and are having some Ethernet issues:As we had problems sourcing the Realtek PHY from the reference design we use the microchip LAN8830T-V/PSA Ethernet PHY which should support Gigabit Ethernet.When...

Schematics.png stefboerrigter_0-1721214588691.png

Specific U-BOOT on STM32MP157-D

Hello,I am currently using the STM32MP157D to develop some tests. It seems that a specific U-BOOT has been developed by ST and flashed in the default factory eMMC.On this specific U-BOOT, some self-test commands are interesting.Could it be possible t...

MJ_TS by Visitor
  • 12 Views
  • 0 replies
  • 0 kudos

RTC TimeStamp enable from RTC Linux Driver

Hello!I'm currently working with a stm32mp157f-dk2 development kit and designing a custom PCB with a STM32MP153A. I have working with the Developer/Distribution package of openST. I want to enable the TimeStamp function of the RTC, and be able to rea...

jutoroa by Associate III
  • 142 Views
  • 1 replies
  • 0 kudos

How to send/receive Ethernet packets in STM32MP157

Hi,I want to send and receive data using Ethernet.I tried this Linux version code, but it didn't works. https://gist.github.com/austinmarton/1922600 After I failed to try, I found this header code, STMMAC.https://git.kernel.org/pub/scm/linux/kernel/g...

inkong by Associate II
  • 1940 Views
  • 2 replies
  • 0 kudos

Problem configuring duty cycle in devicetree

Hello,I am trying to configure a PWM in the boot process. I followed the steps in the documentation https://wiki.st.com/stm32mpu/wiki/TIM_device_tree_configuration .I configured the pwmleds nodepwmleds { compatible = "pwm-leds"; example { labe...

obedPH by Associate III
  • 79 Views
  • 2 replies
  • 0 kudos

Yocto busybox post install failure

I am creating a custom yocto image on a STM32MP157F-DK2. I am using the meta-stm32mp layer as apart of the bitbake build. Yocto version : Scarthgap When I run bitbake I get this failure  ERROR: hydra-image-1.0-r0 do_rootfs: Postinstall scriptlets of ...

qt-kiosk-browser on STM32MP157F-DK2

Hello everyone,For some time I have been trying to launch at least some kind of browser on this platform, better than the one in the example with QtWebKitWidgets.Now I am trying to run Qt Kiosk Browser on my STM32MP157F-DK2 running OpenSTLinux Mickle...

shmonov by Associate
  • 166 Views
  • 2 replies
  • 1 kudos