Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Concurrent external Flash usage when using AI

Good day Folks, Firstly, is it possible to put NN weights on the external Flash, but not use it in memory mapped mode? BSP_XSPI_NOR_Init_t NOR_Init; NOR_Init.InterfaceMode = BSP_XSPI_NOR_OPI_MODE; NOR_Init.TransferRate = BSP_XSPI_NOR_DTR_TRANSF...

exarian by Associate III
  • 903 Views
  • 2 replies
  • 2 kudos

Resolved! STWIN Box Datalog2 WiFi Connection / FTP is not working

Device : STWIN.Box (steval stwbxcs1a) with DATALOG2 3.1.0 firmware. WIFI : Updated the MXCHIP firmware   Objective: Running WiFi connection with APP and/or PnPL messages, Data retrieving with FTP.   Currently this is my application  as viewed in ST B...

WhatsApp Image 2025-10-28 at 11.42.14_66ddbe7a.jpg WhatsApp Image 2025-10-28 at 11.42.16_403e0b50.jpg WhatsApp Image 2025-10-28 at 11.42.29_5d96f471.jpg frogrammer_0-1761650647879.png

Resolved! Connecting STM32n6570-DK with YOLO to train AI - Model

Hi,i'm currently working on a school project with the STM32n6570-DK and I'm pretty new into the STM scene. So my project will mainly be an object detection of different objects. The question is not directly about the STM, it's more about how to imple...

qrmjnn by Associate
  • 827 Views
  • 1 replies
  • 0 kudos

Resolved! NUCLEO-657X0-Q fails to boot and run AI-application

Hey!I'm trying to run my AI model on my NUCLEO-657X0-Q, following @Julian E. great guide in here.I have 2 questions:1. My model has some running issues during booting.In the FSBL code that suppose to jump to the application (JumpToApplication) there ...

amirkfir_0-1762257795857.png amirkfir_1-1762258035776.png
amirkfir by Associate II
  • 641 Views
  • 2 replies
  • 0 kudos

Resolved! Stm32n6570 DK board with AI application

Hi I am using the STM32N6570 with AI application models. I have seen the STM Model Zoo and STM32 AI Services. In the services, the application code is generated automatically based on the model selected from the Model Zoo. My question is: how do I de...

Kumar123 by Associate III
  • 660 Views
  • 1 replies
  • 0 kudos

STM32N6570-DK – Deployment stops when ST-LINK is not connected

Dear STEnvironmentItem Version / Details BoardSTM32N6570-DKOSUbuntu 24.04 LTSPythonConda, Python 3.10STM32AI Model Zoostm32ai-modelzoo-services/object_detectionOperation modedeploymentModelyolov8n_256_quant_pc_uf_od_coco-person-st.tfliteSTM32CubeIDE1...

Vic_Ch by Associate II
  • 1330 Views
  • 7 replies
  • 0 kudos

Resolved! Issue with deploying object detection project on STM32N6-DK

Hello,I am trying to test a deployed application for object detection.I have tested out of the box object detection application code.I can successfully build the project and I can run the code on my board.Unfortunately it doesn't detect any objects. ...

cosard by Associate II
  • 6086 Views
  • 20 replies
  • 2 kudos