cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 6.9.1 and STM32CubeIDE 1.13.1 released.

Ghofrane GSOURI
ST Employee

STM32CubeIDE 1.13.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.9.1 that is available for download.

Main issues fixed in this patch:

This patch release fixes the issues related to the following cases:

STM32CubeMX

  • Ticket 157216: X-Cube-FreeRTOS: compilation Error with IAR.
  • Ticket 157222: CubeMX v6.9 deletes Folder added by user when regenerating the code using MDK-ARM.

Where do I obtain CubeIDE 1.13.1, CLT 1.13.0 and CubeMX 6.9.1?

  1. Updating STM32CubeIDE, the post-update restart fails. STM32CubeIDE must be restarted manually.

Related threads:

CubeMX 6.9.0 Pulls all my custom files from my Kei... - STMicroelectronics Community

1 REPLY 1
Mz.1
Associate III

hi, I'm using STM32H743ZI device with STM32CubeIDE 1.13.1 and  STM32CubeMX v6.9.1.

my project is simple. using only LWIP 

reads and receive UDP packets - nothing else.

when I open Wireshark to see the packets I see nothing:

Mz1_0-1694353501675.png

in older STM32CubeMX version it works.

thank you