Skip to main content
Intector
Senior
February 1, 2025
Solved

STM32CubeMX crash

  • February 1, 2025
  • 3 replies
  • 10893 views

Hello STM,

My STM32CubeMX crashes randomly. I've attached the ioc file so you can run some tests and see for yourself. I tried to make some changes to my original project, and as I reopened the ioc it came up with this message:

Intector_0-1738378509380.png

 

After that, I created a new project and was able to change things around until I activated the XSPI1 and XSPI2 with the Memory Manager and the Memory Loader. After those changes, I got this message:

Intector_1-1738378674728.png

 

I lost all the changes in my project and had to start over. That CubeMX software is annoying. If it's not one thing, it will be another.

My STM32CubeMX version is: 

Intector_2-1738379016368.png

My STM32CubeIDE version is:

Intector_3-1738379089387.png

The attached files are from the test project.

 

 

This topic has been closed for replies.
Best answer by Semer CHERNI

Hello @Intector 

First let me thank you for posting and apologize for the inconveniency.

In fact this is a known issue with the STM32CubeMX 6.13 version which occurs when activating the memory mapping tool (MMT) and Ethernet.

Unfortunately the only solution is either you disactivate the MMT and make the memory settings manually or use STM32CubeMX 6.12.

A permanent fix will be provided in the next STM32CubeMX release which will be published in the near future.

KR,
Semer.

3 replies

Intector
IntectorAuthor
Senior
February 4, 2025

Hello,

I got some updates on the STM32CubeMX crashes. The ioc file contains something like this:

MMTAppReg1.MEMORYMAP.AppRegionName=DTCM
MMTAppReg1.MEMORYMAP.ContextName=Boot
MMTAppReg1.MEMORYMAP.CoreName=ARM Cortex-M7
MMTAppReg1.MEMORYMAP.DefaultDataRegion=true
MMTAppReg1.MEMORYMAP.IPParameters=StartAddress,Size,CoreName,DefaultDataRegion,ContextName,Name
MMTAppReg1.MEMORYMAP.Name=DTCM
MMTAppReg1.MEMORYMAP.Size=65536
MMTAppReg1.MEMORYMAP.StartAddress=0x20000000
MMTAppReg2.MEMORYMAP.AppRegionName=RAM
MMTAppReg2.MEMORYMAP.ContextName=Boot
MMTAppReg2.MEMORYMAP.CoreName=ARM Cortex-M7
MMTAppReg2.MEMORYMAP.DefaultDataRegion=true
MMTAppReg2.MEMORYMAP.IPParameters=StartAddress,Size,CoreName,DefaultDataRegion,ContextName,Name
MMTAppReg2.MEMORYMAP.Name=RAM
MMTAppReg2.MEMORYMAP.Size=465920
MMTAppReg2.MEMORYMAP.StartAddress=0x24000000
MMTAppReg3.MEMORYMAP.AppRegionName=ITCM
MMTAppReg3.MEMORYMAP.Cacheability=WTRA
MMTAppReg3.MEMORYMAP.ContextName=Boot
MMTAppReg3.MEMORYMAP.CoreName=ARM Cortex-M7
MMTAppReg3.MEMORYMAP.DefaultDataRegion=false
MMTAppReg3.MEMORYMAP.IPParameters=StartAddress,Size,CoreName,DefaultDataRegion,ContextName,Name,Cacheability
MMTAppReg3.MEMORYMAP.Name=ITCM
MMTAppReg3.MEMORYMAP.Size=65536
MMTAppReg3.MEMORYMAP.StartAddress=0x00000000
MMTAppReg4.MEMORYMAP.AP=RO_priv_only
MMTAppReg4.MEMORYMAP.AppRegionName=FLASH
MMTAppReg4.MEMORYMAP.Cacheability=WTRA
MMTAppReg4.MEMORYMAP.ContextName=Boot
MMTAppReg4.MEMORYMAP.CoreName=ARM Cortex-M7
MMTAppReg4.MEMORYMAP.DefaultCodeRegion=true
MMTAppReg4.MEMORYMAP.DefaultDataRegion=false
MMTAppReg4.MEMORYMAP.IPParameters=StartAddress,Size,CoreName,DefaultDataRegion,MemType,ContextName,Name,AP,Cacheability,DefaultCodeRegion
MMTAppReg4.MEMORYMAP.MemType=ROM
MMTAppReg4.MEMORYMAP.Name=FLASH
MMTAppReg4.MEMORYMAP.Size=65536
MMTAppReg4.MEMORYMAP.StartAddress=0x08000000
MMTAppReg5.MEMORYMAP.AppRegionName=DTCM
MMTAppReg5.MEMORYMAP.ContextName=Appli
MMTAppReg5.MEMORYMAP.CoreName=ARM Cortex-M7
MMTAppReg5.MEMORYMAP.DefaultDataRegion=true
MMTAppReg5.MEMORYMAP.IPParameters=StartAddress,Size,CoreName,DefaultDataRegion,ContextName,Name
MMTAppReg5.MEMORYMAP.Name=DTCM
MMTAppReg5.MEMORYMAP.Size=65536
MMTAppReg5.MEMORYMAP.StartAddress=0x20000000
MMTAppReg6.MEMORYMAP.AppRegionName=RAM
MMTAppReg6.MEMORYMAP.ContextName=Appli
MMTAppReg6.MEMORYMAP.CoreName=ARM Cortex-M7
MMTAppReg6.MEMORYMAP.DefaultDataRegion=true
MMTAppReg6.MEMORYMAP.IPParameters=StartAddress,Size,CoreName,DefaultDataRegion,ContextName,Name
MMTAppReg6.MEMORYMAP.Name=RAM
MMTAppReg6.MEMORYMAP.Size=465920
MMTAppReg6.MEMORYMAP.StartAddress=0x24000000
MMTAppReg7.MEMORYMAP.AppRegionName=ITCM
MMTAppReg7.MEMORYMAP.Cacheability=WTRA
MMTAppReg7.MEMORYMAP.ContextName=Appli
MMTAppReg7.MEMORYMAP.CoreName=ARM Cortex-M7
MMTAppReg7.MEMORYMAP.DefaultDataRegion=false
MMTAppReg7.MEMORYMAP.IPParameters=StartAddress,Size,CoreName,DefaultDataRegion,ContextName,Name,Cacheability
MMTAppReg7.MEMORYMAP.Name=ITCM
MMTAppReg7.MEMORYMAP.Size=65536
MMTAppReg7.MEMORYMAP.StartAddress=0x00000000
MMTAppReg8.MEMORYMAP.AP=RO_priv_only
MMTAppReg8.MEMORYMAP.AppRegionName=FLASH
MMTAppReg8.MEMORYMAP.Cacheability=WTRA
MMTAppReg8.MEMORYMAP.ContextName=Appli
MMTAppReg8.MEMORYMAP.CoreName=ARM Cortex-M7
MMTAppReg8.MEMORYMAP.DefaultCodeRegion=true
MMTAppReg8.MEMORYMAP.DefaultDataRegion=false
MMTAppReg8.MEMORYMAP.IPParameters=StartAddress,Size,CoreName,DefaultDataRegion,MemType,ContextName,Name,AP,Cacheability,DefaultCodeRegion
MMTAppReg8.MEMORYMAP.MemType=ROM
MMTAppReg8.MEMORYMAP.Name=FLASH
MMTAppReg8.MEMORYMAP.Size=65536
MMTAppReg8.MEMORYMAP.StartAddress=0x08000000
MMTAppRegionsCount=8
MMTConfigApplied=false

After one goes into Tools --> Memory Management settings and turns on the two switches in Code Generation Configuration.

Intector_0-1738697937872.png

 

If you go into the IOC file and delete all the "MMTApp" stuff, STM32CubeMX will usually start. However, all your memory settings will be lost. If you try to activate those switches again, the same thing happens.

 

 

Semer CHERNI
Semer CHERNIBest answer
ST Employee
February 10, 2025

Hello @Intector 

First let me thank you for posting and apologize for the inconveniency.

In fact this is a known issue with the STM32CubeMX 6.13 version which occurs when activating the memory mapping tool (MMT) and Ethernet.

Unfortunately the only solution is either you disactivate the MMT and make the memory settings manually or use STM32CubeMX 6.12.

A permanent fix will be provided in the next STM32CubeMX release which will be published in the near future.

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Intector
IntectorAuthor
Senior
February 10, 2025

Hey @Semer CHERNI 

Thank you for the fast answer. That's exactly what I thought. I edited my linker file and adjusted the MPU settings manually. Since I'm using VisualGDB for development, it's not a big problem. It's just very cumbersome for people using STM32CubeIDE(if there are any) because every time one regenerates the code, all changes are lost.

 

Thank you, and try to keep in mind:

"Always be yourself unless you can be a pirate. Then always be a pirate."