STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ethernet server with Apache2/PHP/MYSQL/PhpMyAdmin (LAMPP)

Hello,I'm currently working into STM32MP157C-DK2 and I have made my own image with the following append:apache2 php phpmyadmin php-cli mysql5But into my internet page (move from //usr/share/.. to another directory) php code didn't work and when I try...

AZAMA by Associate
  • 1056 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP1 complete set of Application Notes availability ?

Hello,I would like to start new design with STM32MP157A in next weeks, but various AppNotes topics, usual for STM32 MCUs was not published, but are mentioned in other AppNotes, exactly:AN5275 - STM32MP1 Series: USB DFU/USART protocols used in bootloa...

weird by Associate II
  • 770 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP1 SOM RGB Parallel

It seems parallel RGB on the MP151 is supported on the TFBGA361 and 448 package.  Is there any manufacturer of SOM modules (preferably DIMM socket based) with a parallel RGB header ?

Resolved! STM32MPU157A-EV1 based board turns off after 17s

Hi everyone, I'm trying to carry the first tests on our STM32MPU157A-EV1 based board but it automatically turns itself off after 17 seconds, what could be the cause of that?It actually allows me to start the SD card flashing process as stated here i...

j_gil by Associate II
  • 1191 Views
  • 6 replies
  • 0 kudos

Has anyone implemented code using Numerical Recipes in C++?

 I've been using some of the routines (numerical integration of ODEs using B-S routine with polynomial extrapolation) for years on Microsoft C++, with great success. However, when I even include the nr.h file, I get errors saying that "template" is a...

LHaze by Associate II
  • 632 Views
  • 2 replies
  • 0 kudos