STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Creating a bootable SD card with dd

I've tried to create a bootable CD card image using both the Starter image as well as a Yocto built image. In both cases the device fails to boot. I've gone into stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/images/stm32mp1 directory and then run:scrip...

nlbutts by Associate II
  • 1701 Views
  • 3 replies
  • 0 kudos

root / ssh is wide open - no password

I connected my STM32MP1 via Ethernet to my network and was surprised that I could ssh root@192.168.x.ywithout a password. No password for root is a security risk. I immediately changed the root password to secure the device. Beware!-- John

JWali by Associate II
  • 555 Views
  • 0 replies
  • 0 kudos

Resolved! STM32MP157C-DK2 won't boot after flashing

I'm able to download an image onto STM32MP157C-DK2 according to the wiki. The Cube Programmer indicates success. When I flip the boot switches to ON and reboot, DL8 lights after a few seconds but nothing on the screen. During flashing the LCD does di...

BMcCa.3 by Associate II
  • 1908 Views
  • 9 replies
  • 0 kudos

Resolved! STM32MP157-DK2: UART7 is not working .

UART7 is not working when configured with same pin numbers as given in the STMCubeMX code.When connected as per schematic pin config, it is working.(Corresponding code also changed)So why is this happening like this? Please help.

USama1 by Associate II
  • 832 Views
  • 2 replies
  • 0 kudos

The DK2 board recording voice is very low volume

Hi, I test the record voice on dk2 board. Using below command to recorded. After recorded, I use aplay to play that file. The sounds volume very low. I had setting some volume through alsamixer command.arecord -f cd -c 2 test.wavDoes it working corre...

SChen.11 by Associate III
  • 749 Views
  • 3 replies
  • 0 kudos