cancel
Showing results for 
Search instead for 
Did you mean: 

Can't access "How to create a layer with device tree files generated via STM32CubeMX" page in Wiki

j_gil
Associate II

Hi,

I'm going through the wiki to try and solve the issues I'm finding on the bring-up of our board.

I found something that could be interesting for me , so from this page I try to access the "How to create a layer with device tree files generated via STM32CubeMX" wiki page, but whe I click on it, I get a "Permission error" and can not see anything.

Is this an error or do I need some kind of special permission?

Kind regards,

j

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
Olivier GALLIEN
ST Employee

Hi @j_gil​ 

This page would have rather displayed "coming soon". Its content is not ready to be shared yet.

In the meantime please share your specific question/concern in order we can help

BR

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
j_gil
Associate II

Thanks for the interest Olivier,

Maybe you saw one other thread of mine where your colleague Patrick suggested me to change what's necessary in the dts so that the u-boot works with an external crystal for the 24MHz clock, instead of an oscillator, which is what the STM32MP157c-EV1 has (Our design is based on this EV1).

So I've been fiddling around the u-boot since then, among the things I've tried here's two:

  1. Change the clk_hse property "st,digbypass;" to "st,css;", which didn't show any changes on the serial output of my system.
  2. Delete the "st,digbypass;" line from the .dtsi, (I inferred this by comparing the generated DeviceTree files by the latest version of the STM32CubeMX from two projects; the first, was just the default configuration of the STM32MP157c-EV1 as it is, and the other one is a modification of the last where I just changed the "High Speed Clock (HSE)" to "Crystal/Ceramic Resonator" under System Core->RCC. This did also not have any effect either.

To be clear, what I've been doing, since I don't want to get deep into manually modifying all the necessary source files, is modifying specific lines of the original U-boot source files (once patched) and then substituting the generated "u-boot-stm32mp157c-ev1-trusted.stm32" for the one in the starter package and then trying to flash as if it were the EV1, with the "FlashLayout_sdcard_stm32mp157c-ev1-trusted.tsv" file.

Thus why I'm interested in the page explaining how to apply the DeviceTree generated by the STM32CubeMX.

It always stops at the same point, same thing it did when I was trying out the EV1 I had which turned out to have an Alpha version of the HW.

Is the a way to find out if the units I have assembled on my board are also Alpha version?

Here's the logs I get (both, from the STM32_Programmer_CLI, and serial communication from the board):

$ STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-ev1-trusted.tsv -tm 20000
      -------------------------------------------------------------------
                        STM32CubeProgrammer v2.1.0                  
      -------------------------------------------------------------------
 
 
 
Warning: Timeout is forced to 20000 ms
 
 
USB speed   : High Speed (480MBit/s)
Manuf. ID   : STMicroelectronics
Product ID  : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN          : 000000000000
FW version  : 0x011a
Device ID   : 0x0500
Device name : STM32MPxxx
Device type : MPU
Device CPU  : Cortex-A7
 
 
Start Embedded Flashing service
 
 
 
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-ev1-trusted.stm32
  File          : tf-a-stm32mp157c-ev1-trusted.stm32
  Size          : 245360 Bytes
  Partition ID  : 0x01 
 
Download in Progress:
[==================================================] 100% 
 
File download complete
Time elapsed during download operation: 00:00:04.027
 
RUNNING Program ... 
  PartID:      :0x01 
Start operation done successfully at partition 0x01
 
Flashlayout Programming ...
[==================================================] 100% 
Running Flashlayout Partition ...
Flashlayout partition started successfully
 
 
Memory Programming ...
Opening and parsing file: u-boot-stm32mp157c-ev1-trusted.stm32
  File          : u-boot-stm32mp157c-ev1-trusted.stm32
  Size          : 754169 Bytes
  Partition ID  : 0x03 
 
Download in Progress:
[==================================================] 100% 
 
File download complete
Time elapsed during download operation: 00:00:11.885
 
RUNNING Program ... 
  PartID:      :0x03 
 
reconnecting the device ...
 
Error: unable to reconnect the target device: time out expired
 
 
Error: Start operation failed at partition 0x03
Error: TSV flashing service failed
NOTICE:  CPU: STM32MP157A?? Rev.A
NOTICE:  Model: STMicroelectronics STM32MP157C eval daughter on eval mother
INFO:    Reset reason (0x15):
INFO:      Power-on Reset (rst_por)
INFO:    Using USB
INFO:      Instance 2
INFO:    Boot used partition fsbl1
INFO:    Product_below_2v5=1: HSLVEN update is
INFO:      destructive, no update as VDD>2.7V
NOTICE:  BL2: v2.0(debug):
NOTICE:  BL2: Built : 13:13:37, Oct  2 2018
INFO:    BL2: Doing platform setup
INFO:    PMIC version = 0x00
INFO:    RAM: DDR3-1066/888 bin G 2x4Gb 533MHz v1.41
INFO:    Memory size = 0x40000000 (1024 MB)
INFO:    BL2 runs SP_MIN setup
INFO:    BL2: Loading image id 4
INFO:    Loading image id=4 at address 0x2fff0000
INFO:    Image id=4 loaded: 0x2fff0000 - 0x30000000
INFO:    BL2: Loading image id 5
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    Receive DFU abort
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    UPLOAD :
INFO:                   Phase ID : 0
INFO:                   address 0x2ffee768
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    UPLOAD :
INFO:                   Phase ID : 0
INFO:                   address 0x2ffee768
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    Start Download partition 0 to address 0xc0000000 length 0
INFO:    USB : DFU : end of download partition : 0
INFO:    Loading image id=5 at address 0xc0100000
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    UPLOAD :
INFO:                   Phase ID : 3
INFO:                   address 0x2ffee768
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    receive request 6
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    UPLOAD :
INFO:                   Phase ID : 3
INFO:                   address 0x2ffee768
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    usb_partition_size: partition size : 0xb80f9
INFO:    Start Download partition 3 to address 0xc0100000 length 753913
INFO:    USB : DFU : end of download partition : 3
WARNING: Skip signature check (header option)
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    UPLOAD :
INFO:                   Phase ID : 0
INFO:                   address 0xffffffff
INFO:    Send detach request
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    Receive Detach
INFO:    Image id=5 loaded: 0xc0100000 - 0xc01b80f9
INFO:    read version 0 current version 0
NOTICE:  BL2: Booting BL32
INFO:    Entry point address = 0x2fff0000
INFO:    SPSR = 0x1d3
INFO:    PMIC version = 0x00
NOTICE:  SP_MIN: v2.0(debug):
NOTICE:  SP_MIN: Built : 13:13:37, Oct  2 2018
INFO:    ARM GICv2 driver initialized
▒ɑ▒*O@2*.▒▒▒▒▒M}qbj▒▒l▒m$J▒Α
'â–’Pâ–’â–’   'â–’2â–’1â–’"
uâ–’H,â–’\â–’â–’â–’%}qâ–’â–’ÙŸ0â–’â–’b).â–’:@â–’1111111mdP

Olivier GALLIEN
ST Employee

Hi @j_gil​ 

Your substitution method is correct but you need also to recompile and update the tf-a in the same way.

Your traces clearly shows you crash during HSE initialization in tf-a

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi Olivier,

I just tried recompiling TF-A also (with the same changes as the U-boot) and still get the same result.

I tried this both, deleting the "st,digbypass" parameter and modifying it to "st,css".

Some values are different but that must be because of the file size variation due to file modifications:

INFO:    usb_partition_size: partition size : 0xb80e0
INFO:    Start Download partition 3 to address 0xc0100000 length 753888
INFO:    USB : DFU : end of download partition : 3
WARNING: Skip signature check (header option)
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    UPLOAD :
INFO:                   Phase ID : 0
INFO:                   address 0xffffffff
INFO:    Send detach request
INFO:    GETSTATUS :
INFO:                   DFU_STATE_IDLE
INFO:    Receive Detach
INFO:    Image id=5 loaded: 0xc0100000 - 0xc01b80e0

Bernard PUEL
ST Employee

Hello,

I see from your trace:

CPU: STM32MP157A?? Rev.A

Public STM32mp1 release is only supporting Rev.B. So I guess you need to update your EV1 board with a new one (MB1262C and MB1263C) or take an hold non public SW release (Beta1 Release).

rgs,

Bernard PUEL
ST Employee

I red all the thread, even if it is on your own design (I did not realized first) the comment above is still valid.

j_gil
Associate II

Thank you Bernard.

While we try to get ahold of release units of the MPU and have them assembled onto a new batch of our boards, can you point out who should I get in touch with in order to have access to he non public Beta1 SW Release?

Kind regards,

j

Bernard PUEL
ST Employee

​As it is not public versions of HW and SW. I would propose to answer offline.