STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DDR3L, bit swap inside bytes. How to configure it ?

i read the following information in the doc AN5122 : Standard fly-by topologyA standard fly-by topology is comprised of:• A distributed A/C bus with 56 Ω on-board termination at VTT (VDD_DDR/2)• A differential clock, distributed to all of the DDR dev...

Resolved! Why is uart0 blocking uart1 ?

Hello,I am running example "OpenAMP_TTY_echo" on the board "stm32mp157c-dk2"I have modified the code a little bit so that channel0 (uart0) doesn't have to wait for a massage from linux side and transmit message every half second. It is sending the me...

IYetk by Associate III
  • 845 Views
  • 2 replies
  • 0 kudos

How to upload Cortex-M4 FW without IDE?

I'm working with Development Kit and want to upload my Cortex-M4 image but I do not want to use IDE. I assume there should be a Linux program that can stop M4, write image into SRAM and restart M4. Where can I find a details on how to do it?Thanks.

dimax by Senior
  • 656 Views
  • 6 replies
  • 0 kudos

How to use Linux RPMSG API on MP1

I'm currently trying to use the Linux API for RPMSG [1]. However, trying to use the example provided in the documentation does not compile (with the OpenStLinux SDK or with my host machine) even though I have the headers installed. Even the sample pr...

RLeve by Associate
  • 1310 Views
  • 4 replies
  • 0 kudos

Resolved! Android repo init error ?

Hi, I try to compile Android on the STM32MP1 following the Wiki and I'm hitting a problem :hico@debian-ha:~/work/st/android$ hico@debian-ha:~/work/st/android$ repo init -u https://github.com/STMicroelectronics/android-manifest -b st-android-9.0.0-201...