DDR3L, bit swap inside bytes. How to configure it ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-10-25 1:51 AM
i read the following information in the doc AN5122 :
Standard fly-by topology
A standard fly-by topology is comprised of:
• A distributed A/C bus with 56 Ω on-board termination at VTT (VDD_DDR/2)
• A differential clock, distributed to all of the DDR devices
– Implement a differential termination of the CLK_N/CLK_P signals using one 100 Ω
resistor.
• There must be a point-to-point connection of the data bus (4 swappable bytes, and
swappable bits in the same byte), including:
– 32 data signal bits (DQ)
– 4 data mask signals (DQMx)
– 4 differential clocks (DQSx_N/DQSx_P)
i would like for the ease of layout swap bit inside byte0 and byte1 of control signals but i dont see any where how to inform the system and set configuration for the bit swap.
Can you point me to a document where it is explain how to setup bit swap configuration ?
Tanks for support
Julien.
- Labels:
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-10-25 5:23 AM
Hello,
you don't need any system configuration when you swap bits inside same byte or even byte Vs byte.
For data, bit and byte numbering on a memory is only a matter of give them unique name, in all cases, you read the bit data on same wire you write it.
This swaps are possible on DDR3/DDR3L as there is no memory register configuration using data lines (configuration uses address/command lanes).
On LPDDR2/LPDDR3, there is some constrains for Byte0 (no bit swap, no byte swap) as it is used to access internal registers.