STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC input protection on STM32MP157C

Hi,I'm interested if there is ADC input protection against voltage transients and overvoltage inside STM32MP157C or I should add external protection for used pins? If I had to add external components do you have some recommendations?Best regards,Nena...

NGajic by Associate III
  • 629 Views
  • 2 replies
  • 0 kudos

Resolved! Changing the eMMC pins with OTP

Hello,I have a custom board based on STM32MP151-C with an eMMC on the following pins:SDMMC2_CK PE3 (AF09)SDMMC2_D0  PE6 (AF07)SDMMC2_CMD   PG6 (AF10)I read that the ROM expects the the SDMMC2_D0 pin on PB14 so I need to change it by using values from...

ANiko.3 by Associate II
  • 3261 Views
  • 10 replies
  • 0 kudos