STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP157-DK2: UART7 is not working .

UART7 is not working when configured with same pin numbers as given in the STMCubeMX code.When connected as per schematic pin config, it is working.(Corresponding code also changed)So why is this happening like this? Please help.

USama1 by Associate II
  • 558 Views
  • 2 replies
  • 0 kudos

The DK2 board recording voice is very low volume

Hi, I test the record voice on dk2 board. Using below command to recorded. After recorded, I use aplay to play that file. The sounds volume very low. I had setting some volume through alsamixer command.arecord -f cd -c 2 test.wavDoes it working corre...

SChen.11 by Associate III
  • 410 Views
  • 3 replies
  • 0 kudos

Resolved! STM32MP1 complete set of Application Notes availability ?

Hello,I would like to start new design with STM32MP157A in next weeks, but various AppNotes topics, usual for STM32 MCUs was not published, but are mentioned in other AppNotes, exactly:AN5275 - STM32MP1 Series: USB DFU/USART protocols used in bootloa...

weird by Associate II
  • 551 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP1 SOM RGB Parallel

It seems parallel RGB on the MP151 is supported on the TFBGA361 and 448 package.  Is there any manufacturer of SOM modules (preferably DIMM socket based) with a parallel RGB header ?