cancel
Showing results for 
Search instead for 
Did you mean: 

Using RAUC with openstlinux

meiss.M
Associate III

We are using rauc to perform remote updates on your target devices.

However, to create the rauc bundle, rauc uses a different image format than the ST image created.

The default imagesource in rauc is:

imgsource = "%s-%s.%s" % (d.getVar('RAUC_SLOT_%s' % slot), machine, img_fstype)

 in file  https://github.com/rauc/meta-rauc/blob/345732f8ef81700e5ca17b4e6a66ae33019cb73b/classes/bundle.bbclass#L197

which I edited to:

imgsource = "%s-%s-%s.%s" % (d.getVar('RAUC_SLOT_%s' % slot), "openstlinux", machine, img_fstype)

What would be the best way to comply with the filenames created by the ST yocto distribution?

What do you suggest?

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
Christophe Guibout
ST Employee

Hello @meiss.M​ ,

The issue comes from stm32 extension files which are not supported by RAUC.

I would recommand to apply the following patch in RAUC :

diff --git a/src/update_handler.c b/src/update_handler.c
index bcd6fd8..c77d7f8 100644
--- a/src/update_handler.c
+++ b/src/update_handler.c
@@ -1520,6 +1520,7 @@ typedef struct {
 RaucUpdatePair updatepairs[] = {
 	{"*.ext4.caibx", "ext4", img_to_fs_handler},
 	{"*.ext4.caibx", "raw", img_to_raw_handler},
+	{"*.stm32", "raw", img_to_raw_handler},
 	{"*.vfat.caibx", "raw", img_to_raw_handler},
 	{"*.ubifs.caibx", "ubivol", img_to_ubivol_handler},
 	{"*.ubifs.caibx", "ubifs", img_to_ubifs_handler},

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
meiss.M
Associate III

Thanks for this, I will try.

Do you recommend using a custom uboot.env script and a copy of the root device?

by adding in st-machine-common-stm32mp.inc :

PARTITIONS_CONFIG[rootfsrauc]  ?= "${IMAGE_BASENAME},rootfs,,${ROOTFS_PARTITION_SIZE},FileSystem"

(after PARTITIONS_CONFIG[rootfs]  ?= "${IMAGE_BASENAME},rootfs,,${ROOTFS_PARTITION_SIZE},FileSystem")

BTF, this is much more convenient in dunfell now.

Greetings, Markus

Christophe Guibout
ST Employee

Hi @meiss.M​ ,

I'am not sure to catch what you want to do : could you please elaborate for which purpose you need to use a custom u-boot env script ?

BTY, you will have to add u-boot-fw-config-stm32mp recipe to you image to allow RAUC to read and write into u-boot env.

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
meiss.M
Associate III

We have built up RAUC with symmetric ROOTFS slots: https://rauc.readthedocs.io/en/latest/scenarios.html#symmetric-root-fs-slots

> BTY, you will have to add u-boot-fw-config-stm32mp recipe to you image to allow RAUC to read and write into u-boot env.

Yes i did this - it works, by patching the thud uboot for adding the respective stm32mp15_trusted_defconfig

Luckily in dunfell it is included, which makes it possible to update the uboot fw env

is this the recommended way to add the additional rootfs :

> PARTITIONS_CONFIG[rootfsrauc]  ?= "${IMAGE_BASENAME},rootfs,,${ROOTFS_PARTITION_SIZE},FileSystem"

Christophe Guibout
ST Employee

Hi @meiss.M​ ,

There is no specific recommended way to add the additional rootfs on STM32MP1.

Nevertheless, a proposition would to build a rootfs image for A, flash this image for both A and B, but you need to run post-install.sh script after flashing B to update partition mount points (kernel cmdline, vendorfs ....). Hope I'am clear enough.

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
meiss.M
Associate III

Hello @Christophe Guibout​ ,

Thank you for your advice,

can you please post me your system.conf

mine looks like this:

# rauc configuration file
 
[system]
compatible=SDM array
bootloader=uboot
statusfile=/boot/raucstatus
 
[autoinstall]
path=/data/fw_update
 
[keyring] 
path=/etc/rauc/ca.cert.pem
 
# [handlers]
# post-install=/sbin/resize-helper # from thud
 
# [slot.bootfs.0]
# device=/dev/mmcblk0p4
# type=ext4
 
[slot.rootfs.0]
device=/dev/mmcblk0p6
type=ext4
bootname=system0
 
[slot.rootfs.1]
device=/dev/mmcblk0p7
type=ext4
bootname=system1

 device=/dev/mmcblk0p7 is the added root device (slot B)

Hello @meiss.M​ ,

Here is mine :

[system]
compatible=stm32mp1
bootloader=uboot
mountprefix=/mnt/rauc
max-bundle-download-size=805306368
 
[keyring]
path=/etc/rauc/ca.cert.pem
 
[handlers]
post-install=/usr/lib/rauc/post-install.sh
 
[slot.rootfs.0]
device=/dev/mmcblk1p13
type=ext4
bootname=A
 
[slot.rootfs.1]
device=/dev/mmcblk1p14
type=ext4
bootname=B
 
[slot.bootfs.0]
device=/dev/mmcblk1p9
type=ext4
parent=rootfs.0
 
[slot.bootfs.1]
device=/dev/mmcblk1p10
type=ext4
parent=rootfs.1
 
[slot.vendorfs.0]
device=/dev/mmcblk1p11
type=ext4
parent=bootfs.0
 
[slot.vendorfs.1]
device=/dev/mmcblk1p12
type=ext4
parent=bootfs.1

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.