STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

On a linux stm32mp157 system can gpio with pullup or pull-down resistors be configured in user space ? If yes how?

I just spent a day trying to configure a gpio with internal pullup using gpiolib. Could not get it configured. Then spent 2 days with device drivers and device trees, and got it working. Seems insane to me that configuring gpios should be this comple...

Rc.1 by Associate II
  • 3606 Views
  • 6 replies
  • 0 kudos

Cannot load STPMIC1 regulate driver

I have a customized STM32MP157AAD board with STPMIC1E PMIC.STPMIC1E is pre-programmed to have same NVM as 1A version.After power up, the board can download firmware by CubeMX and run uboot from SD card, even partially boot the linux kernel.However, t...

uouox by Associate II
  • 719 Views
  • 0 replies
  • 0 kudos