STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB ethernet gadget stops working after replugging cable

Not sure if this is the best forum for this question but I am using the USB OTG port in device mode as ethernet gadget. It works fine if plugged in from boot, or first plug in anytime after. But if unplugged and plugged in again it will not come back...

BillR by Associate III
  • 4350 Views
  • 12 replies
  • 2 kudos

problems setting up codec via the cm4 in engineering mode

I'm trying to set up communication between the codec and the cm4 using the stm32mp157f-dk2 dev board. Debugging in engineering mode.I've set up the gpio, i2c1 and sai2 ports for the CM4 using cubemx, but the code fails when trying to send the require...

KMcev.1 by Associate
  • 424 Views
  • 0 replies
  • 0 kudos

Failed OpenSTLinux flash using STM32CubeProgrammer

Hi all,I have been working with STM32MP157 chipset.I am currently trying to flash the OpenSTLinux to the SDCard using STM32CubeProgrammer inside VMWare.However, it failed in the middle of flashing.Can anyone tell me what I should do?Thank you

DWibo.1 by Associate
  • 567 Views
  • 1 replies
  • 0 kudos

Reduce image size with Yocto

Hello, I've got a board with an STM32 MP CPU and I have to reduce the size of the final image to leave enough space on the NAND memory for a dual rootfs setup. The idea is to remove the alsa layer because I don't need the audio part. I tried to add t...

LLorr.1 by Associate
  • 1194 Views
  • 2 replies
  • 0 kudos

ADC Multiple channel interrupt routine

Hello,I have 7 ADC channel , and its configue as interrupt. But the interrupt each is get generated for different condition how I can check the which ADC channel interrupt is get generated which I have to use the function for distinguish the ADC chan...

MDeva.1 by Associate II
  • 496 Views
  • 1 replies
  • 0 kudos

Resolved! mozjs_60.9.0.bb:do_compile failed with exit code '1 - Cant Compile Distribution Package (SOLVED)

I've followed all the steps from:https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Packagehttps://wiki.st.com/stm32mpu/wiki/PC_prerequisiteshttps://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_PackageCreating openstlinux-5.10-du...

0693W00000BcokoQAB.png 0693W00000BcolgQAB.png

Possible to use STM32MP1 for smart wearable device?

Hi everyone,I am thinking about using STM32MP1 for a smart wearable device, like a smart watch to run some machine learning algorithm. is it possible? is the battery able to support MPU?Does anyone know any product already used STM32MP1? it would be ...

JZhan.24 by Associate
  • 727 Views
  • 2 replies
  • 0 kudos