STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue booting on custom board

I have board based on MB1277 design but on my custom board I'm getting this issue:NOTICE: CPU: STM32MP157AAC Rev.B NOTICE: Model: STMicroelectronics STM32MP157C eval daughter on eval mother INFO: Reset reason (0x15): INFO: Power-on Reset (r...

MBeli.1 by Associate III
  • 2814 Views
  • 7 replies
  • 0 kudos

Resolved! stm32-dwmac: Support of multiple VLAN ids

Hi,we have designed a custom board, based on STM32MP151 and OpenSTLinux 5.10. On this board we use the switch NXP SJA1105S with 3 phys and a MAC-MAC interface between the MPU and the switch. All ports are configured for RGMII mode. At startup(via mod...

CHoll.2 by Associate II
  • 5229 Views
  • 6 replies
  • 0 kudos

Resolved! Hello, I'd like to preserve time after rebooting, when no internet connection is present. Every time I reboot I get the same date, which i presume is the late date there was an internet connection. I'd like to update this system clock with the current tim

root@stm32mp1:~# timedatectl status Local time: Thu 2021-10-14 15:10:06 UTC Universal time: Thu 2021-10-14 15:10:06 UTC RTC time: Sat 2000-01-01 00:00:38 Time zone: UTC (UTC, +0000) System cl...

Lmoio.1 by Senior
  • 4829 Views
  • 5 replies
  • 0 kudos

Resolved! WiFi Module choice for STM32MP15

Hi,On the DK2 board, there is a LBEE5KL1DX-883 from Murata. But I want to use their LBEE5HY1MW (Type 1MW - LBEE5HY1MW | Wi-Fi® Modules / Wi-Fi® + Bluetooth® Modules | Murata Manufacturing Co., Ltd.) in my design. But on their site, they only mentions...

In STM32mp157f-dk2 board on sdmmc2 and sdmmc3 getting different throughput over SDIO even though DT configuration is same for both the sdmmc controller.

In STM32mp157f-dk2 board, sdmmc2 is used for inbuilt wifi over SDIO and I am using sdmmc3 with esp32 chip to connect it to wifi over SDIO. I am able to connect ST board to wifi over sdmmc3 but with iperf it is giving constant throughput of 1 Mbps irr...

SR.11 by Associate
  • 1064 Views
  • 0 replies
  • 0 kudos

How do I get U-Boot to detect a single quad-SPI memory so that I can program it with STM32CubeProgrammer?

Hi. I'm using the v2.1.0 ecosystem to build for a target that will boot TF-A & U-Boot from a single ISSI IS25LP016D-JNLE 2 mebibyte quad-SPI NOR flash connected with the rest of the system in e.MMC. (This is to work around the bug in the rev.B STM32M...

Spamfast by Associate II
  • 3207 Views
  • 2 replies
  • 0 kudos