STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

In STM32mp157f-dk2 board on sdmmc2 and sdmmc3 getting different throughput over SDIO even though DT configuration is same for both the sdmmc controller.

In STM32mp157f-dk2 board, sdmmc2 is used for inbuilt wifi over SDIO and I am using sdmmc3 with esp32 chip to connect it to wifi over SDIO. I am able to connect ST board to wifi over sdmmc3 but with iperf it is giving constant throughput of 1 Mbps irr...

SR.11 by Associate
  • 1090 Views
  • 0 replies
  • 0 kudos

How do I get U-Boot to detect a single quad-SPI memory so that I can program it with STM32CubeProgrammer?

Hi. I'm using the v2.1.0 ecosystem to build for a target that will boot TF-A & U-Boot from a single ISSI IS25LP016D-JNLE 2 mebibyte quad-SPI NOR flash connected with the rest of the system in e.MMC. (This is to work around the bug in the rev.B STM32M...

Spamfast by Associate II
  • 3273 Views
  • 2 replies
  • 0 kudos

IOTA on STM32MP157DK-2

Is it possible to use the STMCUBE expansion for IOTA on STM32MP157DK-2 or is there anyway to use IOTA client libraries.I tried installing the Python library but it would not install.I have the STM32CubeExpansion_IOTA1_V2.0.0 but do not know how to ru...

ADesh.6 by Associate
  • 2064 Views
  • 3 replies
  • 0 kudos

Resolved! Using mmap in C-Code from Linux application to access GPIOs. I want to control the GPIO PF4 on the STM32MP1 with mmap() due to speed requirements, but the pin is not toggling.

Details:HW: Phytec Sargas Board, which is similar to the STM32MP1-DK2.Build environment: Cross compiling with SDK generated by Yocto.Linux: Yocto build, based on st-image weston.Device Tree configuration: As far as I understood not needed to access s...

Led by Senior
  • 9297 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.