2021-04-27 2:47 AM
Hi,
I'm developping an application where we want the cortex-M doing some power management (with OpenAMP) and the cortex-A taking picture and saving it on SD card.
I have the STM32MP157A-EV1.
I used the OpenAMP_TTY_echo_wakeup sample that I modified for my need to do the power management. Everything is working fine if I boot in third mode (ie. stm32mp157c-ev1-m4-examples). However, I don't have any camera input as it's saying that /dev/video0 doesn't exist.
If I boot in second mode (ie. stm32mp157c-ev1-a7-examples), I've got a camera but I couldn't suspend at first (systemctl suspend), because I would get the following error :
PM: Device 40017000.dac:dac@1 failed to suspend: error -16So, I commented every line of code linked to DAC and it worked (ie. I could have the OpenAMP and camera running at the same time). But it's not that great of a workaround. Ideally, I would want to update the device tree. Where could I find the initial device trees used so that I just can quickly modify them ?
I know they are stored in <path>/Developer-Package/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/linux-5.4.56/arch/arm/boot/dts but I think it's the default one and I would like the stm32mp157c-ev1-m4-examples.dts and stm32mp157c-ev1-a7-examples.dts to make these minimal changes.
Note : I tried to get the dts from the /boot/dtb with dtc command but it's saying me there is a syntax error.
Best regards !
Solved! Go to Solution.
2021-04-27 8:46 AM
Hi @AHayo.1 ,
stm32mp157c-ev1-m4-examples.dts and stm32mp157c-ev1-a7-examples.dts are indeed in the <path>/Developer-Package/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/linux-5.4.56/arch/arm/boot/dts ... once you have applied the ST patches.
Refer to README_HOW_To file in <path>/Developer-Package/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0 for complete installation of sources.
Hope it help,
Olivier
2021-04-27 8:46 AM
Hi @AHayo.1 ,
stm32mp157c-ev1-m4-examples.dts and stm32mp157c-ev1-a7-examples.dts are indeed in the <path>/Developer-Package/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/linux-5.4.56/arch/arm/boot/dts ... once you have applied the ST patches.
Refer to README_HOW_To file in <path>/Developer-Package/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0 for complete installation of sources.
Hope it help,
Olivier
2021-05-03 1:00 AM
Yes, thank you very much !
Nice day !