STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

We would like to use the USART1 in our design but the device is not available later under /dev/ttySTM. In the kernel log it seems that the device is registered but then the serial0 seems to use ttySTM1 and you do not have that interface available.

[   0.056781] Serial: AMBA PL011 UART driver[   2.010824] stm32-usart 40010000.serial: interrupt mode for rx (no dma)[   2.010858] stm32-usart 40010000.serial: interrupt mode for tx (no dma)[   2.010901] 40010000.serial: ttySTM0 at MMIO 0x40010000 (i...

MEnge.3 by Associate II
  • 1874 Views
  • 2 replies
  • 0 kudos

Resolved! STM32-CRC module build issue.

Hi all,I have been trying to build a custom machine based on STM32MP157C MPU. Right now I am facing a weird issue.Defconfig file is attached. However upon giving build , i cannot see the stm32-crc module , built added and loaded. Is there something w...

NPal.2 by Senior
  • 3825 Views
  • 3 replies
  • 0 kudos