STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Could someone help me with some documentation on the configuration of watchpoints in STM32MP157A board?

I was working on the STM32MP157A-DK1 board which has Cortex-A7 + Cortex-M4 processors. I wanted to configure the watchpoints present specifically on the Cortex-A7 processor via C code. The Cortex-A7 technical reference manual indicates the use of MRC...

STM32MP1 Timer

Hi all,I was wondering whether we can achieve a PWM frequence of 1-3Hz with the existing timer which we have. I am targeting to generate a PWM signal within the same frequency range but using A7 as primary.How can we achieve that ?? I do have some id...

NPal.2 by Senior
  • 1385 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to set DDR clock

Hello,I am having a hard time setting the DDR clock at pll2 for an stm32mp157.The clock has been configured to 528MHz using CubeMX. I checked cfg for pll2 in the DeviceTree against the Datasheet / Referance Manual and all settings seem correct.Yet /s...

jvog.sen by Associate II
  • 2867 Views
  • 3 replies
  • 0 kudos

Dear ST Community, I am working on a project using STM32MP157D-DK1. I'm specifically working on interprocessor communication between the M4 and A7 cores.

I followed the guide from the following ST's video: https://www.youtube.com/watch?v=PsiFDHH87vo&t=407s In the guide, the A7 core is initiating the communication. I have been playing with the code to make M4 the one to initiate the communication, but ...

k44 by Associate II
  • 1284 Views
  • 1 replies
  • 0 kudos