STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157-DK2 Ethernet

Hi, I can't to connect my board by ethernet connector, when I connect the cable both leds are always off. I try using ifconfig to set a ip but my board doesn't respond to ping request, but when I used ifconfig to set ip over usb0 my board respond to ...

ECaba by Associate II
  • 2128 Views
  • 2 replies
  • 0 kudos

Can't Debug in Engineering Mode using STM32MP157-DK2. OpenOCD Error: Could not find MEM-AP to control the core

Trying to create a simple application that will toggle LD9 in Engineering Mode but get an error with the OpenOCD.Output on console window is as follows:Open On-Chip Debugger 0.10.0+dev-01124-gbfb41e6 (2018-11-16-15:23) Licensed under GNU GPL v2 For b...

BMcCa.3 by Associate II
  • 3155 Views
  • 3 replies
  • 0 kudos

Resolved! The new ANA0 / ANA1 pins

Hi,I'm currently figuring out about the new ANA0 / ANA1 pins.As far as I understand, those pins are always connected to the ADC so that I don't need to touch the GPIO registers in order to use those pins. Is my understanding correct?Also I can connec...

0690X000009Ymq4QAC.png

Resolved! Slightly confused about IPCC peripheral

I have a STM32MP157C-DK2, and I'm interested in better understanding how the IPCC peripheral works. I've tried out the OpenAMP echo example and trawled through its code, and the associated HAL code. I have generally completely avoided the HAL for mic...

unicycle by Associate III
  • 1604 Views
  • 1 replies
  • 0 kudos