cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157F-DK2 support in mainline (vanilla) U-Boot

krjdev
Associate II

Are there any plans to support the STM32MP157F-DK2 board in mainline (vanilla) U-Boot?

It's supported in the ST fork from U-Boot, but with an older version from U-Boot from the year 2020.

Could also ask this in the U-Boot mailing list.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Kevin HUBER
ST Employee

Hello @krjdev​ ,

The support of the mainline U-Boot is not planned for the moment.

I will come back to you if I have more information.

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here