STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! question about ecosystem4

Hi,I follow "https://wiki.st.com/stm32mpu/wiki/PMIC_hardware_components#Support_in_Cortex-A7_Secure" can port the ecosystem 3.0 on the kit "stm32mp157c-odyssey" successfully, but fail to port the ecosystem4.0.The error log is :" 14:13:55 : Start Embe...

zqizh.1 by Associate III
  • 3243 Views
  • 1 replies
  • 0 kudos

Stm32mp157a kernal booting issue

Hi,We are using stm32mp157a processor in my custom board.I have download stm32mp157a-dk1 discovery kit code.The difference between discovery board and my custom board is Debug Serial port Configuration.In Discovery Board The debug uart pins are PG11-...

Resolved! ENABLE_PARTITIONS_IMAGE not enabled

When I change the download directory for my yocto project in my local.conf file, this note pops up, what is this and should I do anything about it.NOTE: /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/meta-st/met...

Gencay by Associate III
  • 2711 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP1) How to add HDMI extra mode?

Hello everyone ~​My custom board has RGB(LTDC) and HDMI display interfaces. We want to display same screen on same time.(duplicate mode)So, LTDC interface connected to local LCD and HDMI transmitter(sii9022).&ltdc node of my dts is below ..&ltdc{ pi...

0693W00000QNNNwQAP.png 0693W00000QNNOQQA5.png