STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I was following this how to create your own machine tutorial and got this warning and my flash_layout directory is empty.

Link to the tutorial and warning:WARNING: st-image-weston-1.0-r0 do_st_write_license_create_summary: IMG LIC SUM: File does not exist with open file /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxwesto...

Gencay by Associate III
  • 3598 Views
  • 5 replies
  • 0 kudos

Currently compiling Distribution Package with meta-flutter and meta-clang layers, binutils-native-2.38-r0 do_fetch task running for 3 hours and it is only at %76 percent. Why is this task takes a lot of time?

I did a repo sync to see if there are new version but did not worked after I stopped compiling, started again and it began where it left but moving really slow that particular task.

Gencay by Associate III
  • 890 Views
  • 0 replies
  • 0 kudos

Resolved! When issuing the shutdown command the BUCK3 VDD regulator used for IO is not turned off.

When we tried the shutdown command ( shutdown -hP now ) from the debug console, all the PMIC regulators are turned off, except for the BUCK3 VDD regulator used for IO.Both our custom board which uses STPMIC1E and the STM32MP157F-eval board which has ...

SKris by Associate III
  • 2071 Views
  • 2 replies
  • 0 kudos