cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP1 public key hash (OTP WORD 24 to 31)

mikefae
Associate
  1. Is it possible to use OTP WORD 24 to 31 without enable security boot with STM32MP1 part numbers which didn't has security boot option like STM32MP157A/D?
  2. Same as above but with STM32MP1 part numbers which has security boot option like STM32MP157C/F?
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi @mikefae​ 

See note 3 of Table 17 in RM0436 Rev.6

In addition to Reference Manuel, the datasheet ordering information will tell you which device has secure-boot option (here STM32MP15xD or F could fit your needs).

Regards,

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

4 REPLIES 4
OlivierK
ST Employee

Hi mikefae (Community Member)

As long as authentication is not used, it is possible to use OTP 24-31 for other purposes.

Regards,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
OlivierK
ST Employee

Just one precision on STM32MP157A/D parts, OTP24-31 are permanently write locked on devices without secure-boot option as specified in the Reference Manual. So the above it is only possible on C/F parts.

Regards,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
mikefae
Associate

Hello Olivier,

Thank you for your support.

May we know where can find more information about OTP24-31 are permanently write locked on devices without secure-boot option in the reference manual?

PatrickF
ST Employee

Hi @mikefae​ 

See note 3 of Table 17 in RM0436 Rev.6

In addition to Reference Manuel, the datasheet ordering information will tell you which device has secure-boot option (here STM32MP15xD or F could fit your needs).

Regards,

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here