cancel
Showing results for 
Search instead for 
Did you mean: 

How do I configure an stm32mp157c GPIO pin to output?

GeorgeR
Associate II

I have configured the pins for uart7 to communicate with our zwave chip.

in kernel-source/arch/arm/boot/dts/stm32mp157c-dk2.dts

&uart7{
        pinctrl-names = "default", "sleep";
        pinctrl-0 = <&uart7_pins_a>;
        pinctrl-1 = <&uart7_sleep_pins_a>;
        status = "okay";
 
        zwave {
                uart7-gpios = <&gpioi 5 GPIO_ACTIVE_LOW>,
                              <&gpioi 7 GPIO_ACTIVE_LOW>,
                              <&gpioc 7 GPIO_ACTIVE_LOW>;
        };
        /* USER CODE BEGIN uart7 */
        /* USER CODE END uart7 */
};

kernel-source/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi :

        uart7_pins_a: uart7-0 {
                pins1 {
                        pinmux = <STM32_PINMUX('A', 15, AF13)>; /* UART7_TX */
                        bias-disable;
                        drive-push-pull;
                        slew-rate = <0>;
                };
                pins2 {
                        pinmux = <STM32_PINMUX('E', 7, AF7)>; /* UART7_RX */
                        bias-disable;
                };
        };
 
        uart7_sleep_pins_a: uart7-sleep-0 {
                pins {
                        pinmux = <STM32_PINMUX('A', 15, ANALOG)>, /* UART7_TX */
                                 <STM32_PINMUX('E', 7, ANALOG)>; /* UART7_RX */
                };
        };

I want to control the chip with three output GPIO pins (C7, I5, and I7).

When I bitbake this and load it on the board, the configuration does not change. For C

# gpiodetect
gpiochip0 [GPIOA] (16 lines)
gpiochip1 [GPIOB] (16 lines)
gpiochip2 [GPIOC] (16 lines)
gpiochip3 [GPIOD] (16 lines)
gpiochip4 [GPIOE] (16 lines)
gpiochip5 [GPIOF] (16 lines)
gpiochip6 [GPIOG] (16 lines)
gpiochip7 [GPIOH] (16 lines)
gpiochip8 [GPIOI] (12 lines)
gpiochip9 [GPIOZ] (8 lines)

gpiochip2 - 16 lines:
        line   0:      unnamed       unused   input  active-high
        line   1:      unnamed       kernel   input  active-high [used]
        line   2:      unnamed       kernel   input  active-high [used]
        line   3:      unnamed       unused   input  active-high
        line   4:      unnamed       kernel   input  active-high [used]
        line   5:      unnamed       kernel   input  active-high [used]
        line   6:      unnamed       unused   input  active-high
        line   7:      unnamed       unused   input  active-high
        line   8:      unnamed       kernel   input  active-high [used]
        line   9:      unnamed       kernel   input  active-high [used]
        line  10:      unnamed       kernel   input  active-high [used]
        line  11:      unnamed       kernel   input  active-high [used]
        line  12:      unnamed       kernel   input  active-high [used]
        line  13:      unnamed       unused   input  active-high
        line  14:      unnamed       unused   input  active-high
        line  15:      unnamed       unused   input  active-high

and I

gpiochip8 - 12 lines:
        line   0:      unnamed       unused   input  active-high
        line   1:      unnamed       unused   input  active-high
        line   2:      unnamed       unused   input  active-high
        line   3:      unnamed       kernel   input  active-high [used]
        line   4:      unnamed       unused   input  active-high
        line   5:      unnamed       kernel   input  active-high [used]
        line   6:      unnamed       kernel   input  active-high [used]
        line   7:      unnamed       kernel   input  active-high [used]
        line   8:      unnamed       kernel   input  active-high [used]
        line   9:      unnamed       unused   input  active-high
        line  10:      unnamed       unused   input  active-high
        line  11:      unnamed  "interrupt"   input  active-high [used]

Where and how can I change the GPIO pins?

Can I change them in the kernel-source/arch/arm/boot/dts/stm32mp157c-dk2.dts and/or in kernel-source/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi ?

Thanks in advance,

George

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
PatrickF
ST Employee

Hi @GeorgeR​ 

I'm not expert, but you should probably need to declare a driver in your 'zwave' section (something like "compatible = ....").

Or use a dummy device (i.e. no driver)

https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_kernel_space

Otherwise, without specific driver nor any DT, you could control any 'free' GPIO:

https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_userspace

This method could be used from any code (e.g. C or python), see also https://community.st.com/s/question/0D53W00001UZllVSAT

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
GeorgeR
Associate II

Thank you @PatrickF​, I will check out the information.

Regards,

@GeorgeR​