STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP157 SDcard level shifter

Hi guys,The schematics for STM32MP15x-EVAL board (MB1263) uses a level shifter for SDcard from NXP (IP4856CX25) that is now obsolete. I found 2 close alternatives:ST6G3244MEBJR from ST, with one pin only (C4) different from IP4856TXS0206YFPR from TI,...

NCF by Associate II
  • 6284 Views
  • 7 replies
  • 0 kudos

Resolved! STM32MP15 ECO 5.0.0. kernel halts after Secondary CPU 1 switching to normal world boot

Custom board. Boot log as belowextlinux.conf:MENU BACKGROUND /splash_landscape.bmpTIMEOUT 20LABEL OpenSTLinuxKERNEL /uImageFDTDIR /INITRD /st-image-resize-initrdAPPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=${console},...

Resolved! STM32MP157 - memory for the M4 core

Dear experts. ​we plan to use a STM32MP157, where the A7 core should have 512MB DDR RAM, and theM4 core 16 MB. What options exists, to give the M4 core that 16 MB of RAM?From the DS, i understand that the DDR RAM of the A7 is not accessible for the M...

Resolved! OPTEE backwards compatibility

Hi,We are using the meta-st-stm32mp layer in out Yocto build system. We have had the system run on the Dunfell distribution up until now with OPTEE as the secure OS.For Dunfell the version of OPTEE is 3.12 along with patches from ST, a we tried to up...