STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is the highest version of opencv compatible with the gstreamer library included in this SDK?

I have transplanted the latest opencv-4.8.1 on the STM32MP135F-DK Discovery Board and run a program to capture video stream from a camera on the borad.I found if I cmake the opencv-4.8.1 source code with "-DWITH_GSTREAMER=ON -DBUILD_GSTREAMER=ON",and...

babai50 by Associate
  • 3073 Views
  • 1 replies
  • 0 kudos

Resolved! change OpenST Linux version in STM32CubeMX

We are using developBoard by Emcraft with STM32MP157A.Emcraft release board with Openstlinux 4.14. If I want change devicetree of STM32MP1 i need use STM32CubeMX to export new devicetree.If i go in STM32CubeMX-->Project Manager-> Project OpenSTLinux ...

AApol.3 by Associate
  • 4744 Views
  • 5 replies
  • 0 kudos

STLINK-V3PWR feedback

Not sure if this is the right place to write this, but I cannot help to write:- STLINK-V3PWR is a great tool.- I wish it had an external power input other than USB-C. It may be common in some computer setups, but powered USB ports might be challengin...

mete by Senior II
  • 2269 Views
  • 1 replies
  • 3 kudos

Resolved! How do I open a uboot shell?

I know this is probably a really stupid/noob question but I was trying to flash the STM32MP157D-DK1 board I have for the first time following the following guide:https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package I ran into ...

JayDev by Senior II
  • 12102 Views
  • 10 replies
  • 0 kudos

STM32MP157F-DK2 Dual ADC with DMA

Dear all,I'm currently using the STM32MP157F-DK2 series, and I'm trying to use the ADC1 and ADC2 in dual regular simultaneous mode triggered by TIM2 out event. Also, I used one DMA stream (DMA2_stream0) to read the ADC values of the Common Data Regis...

image_2023-09-21_165417637.png
jutoroa by Associate III
  • 9065 Views
  • 4 replies
  • 0 kudos