ST25 NFC/RFID tags and readers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST25R3916 External field detector

Hello Support team,@Travis Palmer We are working on the ST25R3916 NFC-based product.We are facing the issue of high power consumption during NFC active scanning operation so, we want to start the NFC active scanning mode on the External field detecto...

ChintaN1 by Associate III
  • 998 Views
  • 3 replies
  • 0 kudos

Resolved! STEVAL-SMARTAG2 - Error: failed to erase memory

I am trying to update the firmware in the STEVAL-SMARTAG2 using Memory & File editing  in STM32 CubeProgrammer Windows Application., but I get Error: failed to erase Memory.My goal is to install your demo firmware to use the SMARTAG2 with ST NFC Sens...

Screenshot (3073).png Screenshot (3075).png Screenshot (3076).png IMG_0292.jpg
VColi.1 by Associate II
  • 933 Views
  • 3 replies
  • 1 kudos

Resolved! Get sensor Reading via RF on STEVAL-SMARTAG1

I've got a STEVAL-SMARTAG1, and i need to build a React Native App that reads the sensor reading stored in the memory via RF.To do so i'm using "react-native-nfc-manager" library to use the NFC sensor on the phone to read TagData but that doesn't con...

Albi by Associate
  • 864 Views
  • 1 replies
  • 0 kudos

Resolved! How to use TruST25 without being approved for AN5580?

Hey,I recently bought ST25-TAG-BAG-UI1 and hoped I could experiment with it for a specific application but I soon realized there is no documentation available publicly. I've applied for access to AN5580 but my application got rejected (I guess becaus...

taday by Associate
  • 1071 Views
  • 3 replies
  • 0 kudos

ST25R3911 gpio interrupt

I have integrated the ST25R3911B into a Linux development board, using spi+gpio for communication.I currently have GPIO configured for edge-triggering (both), and I am polling for card readings at a frequency of 300ms.However, I've noticed that the G...

zhaocz by Associate II
  • 550 Views
  • 1 replies
  • 0 kudos

Resolved! cant reproduce image uploading function through the app compiled from the ST source code(STSW-ST25I)

Dear Sir      We are developing an iOS mobile application software. We downloaded the official source code of ST and compiled the app we need.When verifying the development board, we encountered the following problems: the ST official app(STSW-ST25IO...

ivanT by Associate II
  • 1096 Views
  • 3 replies
  • 0 kudos