ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! read maximum data from st25tv16k

Hi,Reader IC - ST25R3916RFAL version - 2.8.0Serial interface - I2CI am trying to read the entire memory (2KB) from ST25tv16k using the api rfalNfcvPollerExtendedReadMultipleBlocks.eg:-  err = rfalNfcvPollerExtendedReadMultipleBlocks(flags, NULL, bloc...

andy_long_2-1708177876605.png andy_long_1-1708177783756.png
andy_long by Associate III
  • 993 Views
  • 3 replies
  • 1 kudos

Resolved! ST25R3917 doesn't commnicate on the I2C

ST25R3917 doesn't commnicate on the I2C (Address 0x50) it seems like the chip doesn't start. Maybe a problem with the crystal?- Drawn current is 50uA- Signal on MCU_CLK is a 32.5kHz Squarewave- IRQ line stays lowI assume that the capacitance on the 2...

Resolved! Errata RFAL

Hi,Do you have an errata document for the RFAL library ? How can the customers know if there is an updated RFAL library ?Best regards,

Luke_abc by Associate III
  • 900 Views
  • 2 replies
  • 1 kudos

Resolved! ST25DV04KC - how to read NDEF Text from I2C?

We're evaluating the ST25DV04KC for our application. We want to write to the ST25DV04KC from NFC and read the info from I2C from our MCU.We're able to use NFC app on the smart phone to write an NDEF Text of "12345". We can read it via NFC. But readin...

dzuy by Associate II
  • 2595 Views
  • 10 replies
  • 4 kudos

Resolved! Issue with I2C communication with ST25DV64KC tag

Hi @Rene Lenerve  @JL. Lebon  @Brian TIDAL So basically I am connecting ST25DV64KC tag with MKE14F512VLL16 based controller and I want to write on the tag through i2c but as I am sending data using I2c write and as I am checking using Logic analyzer ...

PoolBear by Associate III
  • 3284 Views
  • 15 replies
  • 6 kudos

Resolved! ST25DV64KC RF SWITCH ON/OFF

Hi Community,I´m trying to import this driver for my custom board,fp-sns-stbox1/Drivers/BSP/Components/st25dvxxkc/st25dvxxkc.c at main · STMicroelectronics/fp-sns-stbox1 (github.com)could someone explain this more? why should NULL be written in ICREF...

Danny0007_1-1707663840703.png

Resolved! ST21NFCD_Application_Tool

Hi, we are using ST21NFCD in one of our wearable products. I am referring to the document: "AN_21NFCD_Antenna_Matching_RF_Config Rev 7" to know about the NFC antenna design and tuning. It is mentioned here about the application tool used for impedanc...

Resolved! LL driver for reading register of ST25DV64KC

Hi community,since I cannot find a suitable LL-driver for reading register with 16bits address, here is my experiment.the nfc tag init function: the ReadID funciton is called, in background is GetICREF function.in low level the BSP_I2C2_Read16 functi...

Danny0007_3-1707670881254.png Danny0007_1-1707670564641.png Danny0007_0-1707670333905.png Danny0007_4-1707670999633.png

Resolved! Can not detect a T5T tag with x-nucleo-nfc03a1

Hi, I am having some problems with my inplementation.Here is my scenary: + I am using a STEVAL-SAMARTAG1 with one shot mode example code, as my T5T tag. + I am using a NUCLEO-F722ZE board with x-nucleo-nfc03a1 as my NFC reader. My first problem is th...

sofiabv by Associate
  • 1208 Views
  • 3 replies
  • 0 kudos