There is a newly introduced bug in the freshly upgraded package coming with the IDE 1.11. MX_SDMMC1_SD_Init(void) does not configure hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B but directly to the final state choosen in CubeMX (in my case 4B). But the SD r...
Hi @Pavel A. When I create a new project with HSE/4, there is no definition of HSI_VALUE in the project properties as long as I generate with the HAL drivers. After a switch to LL drivers in CubeMX and a generation, the .mxproject AND the project pro...
Hello everyone,This topic is 8 year old but I just discovered that the issue is back ! The HSI_VALUE is forced to 4MHz in the compiler command line options, instead of 16MHz (defined correctly in the template code file, but cut out by a #ifndef...). ...
Hello,I confirm the issue, in my case regenerating the project configuration inside STM32CubeIde deletes my custom files in Core and Middleware directories.