Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L052 external interrupt issue?

STM8L052XX – External interrupt on same pin number with different ports (PC0 & PF0)I am using STM8L052R8T6.I have already configured an external interrupt on PC0 (PORTC, pin 0).Now I want to configure an external interrupt on PF0 (PORTF, pin 0) as we...

Glodhi by Associate II
  • 388 Views
  • 1 replies
  • 1 kudos

Resolved! M95P16I write cycle calculation?

I'd like to know about the write cycle for the m95p16i EEPROM.I'm using "Page write (02h)" to write 32 bytes to page 0.The first write is to address 00h, the second to address 21h.I continue to write 32 bytes at a time, writing 16 times until the las...

STM8S103f3 interrupt

Dear ST team, STM8S103f3   I need to initialize interrupt but how I can define particular pin of the port for interrupt .Or how to initialize two interrupt in one port.please share example or library   RM0016thanks and regardsGuddu  

Glodhi_0-1767244137138.png Glodhi_1-1767244178968.png
Glodhi by Associate II
  • 622 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F103C8T6 Bluepill Issue with CubeIDE

Hi Team,I was working on STM32F103C8T6 Bluepill board. I was using this board with ST-LinkV2 to connect with CubeIDE. When i tried to flash a sample LED blink program via CubeIDE, it gave an error saying 'Target not found'. But at the same time i was...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.