cancel
Showing results for 
Search instead for 
Did you mean: 

pinout diagram for a green "Black Pill" ?

jstor.1the lost one
Associate II

I have a black pill, but board is green in color, chip says stm32f401ccu6, 44pin.

where can i get a pinout diagram for this board, ?

only blackpill boards pinouts that I can see are the newer 40 pin boards

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

It took about 30 seconds to find this hit:

https://stm32-base.org/boards/STM32F401CCU6-WeAct-Black-Pill-V1.2.html

Note that stm32f401ccu6 is 48 pins, not 44.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Super User

It took about 30 seconds to find this hit:

https://stm32-base.org/boards/STM32F401CCU6-WeAct-Black-Pill-V1.2.html

Note that stm32f401ccu6 is 48 pins, not 44.

If you feel a post has answered your question, please click "Accept as Solution".

The GREEN board is 44 pins vs the BLACK board being 40 pins.  There may be an actual nice color graphic pin out of the GREEN board, but I have also not been able to locate it, either.

https://stm32-base.org/boards/STM32F401CCU6-STM32-Mini-F401

Yes, the stm32f401 processor chip is 48 pins.

note there is an error, that header should list 22x1 vs 20x1

 

You realise you're replying to a 5-year-old post?

But the moral of the story remains: make sure you can get adequate documentation before you part with any money!

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.