cancel
Showing results for 
Search instead for 
Did you mean: 

NB-IoT board

celika
Associate

Hello,

I'm working on a project that requires the implementation of NB-IoT and to do this I started by testing the Discovery Kit B-L462CELL1, which is very poorly documented. I also noticed that the LBADXX1SC modem used by the kit is now obsolete.

Can you recommend a development board from ST Microelectronics that would enable me to do NB-IoT (with zephyr would be a plus)?

Thanks in advance.

1 ACCEPTED SOLUTION

Accepted Solutions

Did you see my update - LBADXX1SC doesn't actually seem to be obsolete?

As I said any module or board should be usable - just find one which suits your requirements.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

View solution in original post

3 REPLIES 3
Andrew Neil
Super User

Does it really need to be a board from ST ?

Even with the B-L462CELL1, the NB-IoT module is 3rd-party (Murata).

Generally, such modules are controlled via AT commands - so, once you can do AT commands, you can use any module...

 

PS:

 


@celika wrote:

I also noticed that the LBADXX1SC modem used by the kit is now obsolete.


Not according to Murata's site?

AndrewNeil_0-1743499323689.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Not necessarily a board from ST. If you have another module or board to advise me, I'm interested.

Did you see my update - LBADXX1SC doesn't actually seem to be obsolete?

As I said any module or board should be usable - just find one which suits your requirements.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.